GEX7903902-00

RS-485 configuration

Before connecting your device to the RS-485 bus, use the meter’s display, or ION Setup to configure your meter’s default RS-485 settings.

Your meter has one RS-485 connection.

Your meter must have a unique unit identifier (address) and have the following settings match the rest of the devices on the RS-485 bus:

  • Protocol

  • Baud rate

  • Parity

You can use a communications converter (USB to RS-485 or RS-232 to RS-485) to connect to your meter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?