GEX7903902-00

HMI setup

HMI setup enables you to configure contrast, backlight time-out and password parameters.

The meter’s display screen and buttons allow you to navigate and edit the required parameters.

To enter into HMI Setup:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Setup.
  4. Press OK.
  5. Enter the password. Default password is 0000.
  6. Use Up or Down button to navigate to HMI Setup.
  7. Press OK to enter HMI Setup.
  8. Press Left button to exit HMI Setup.
The navigation of HMI setup:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?