RMS page
To view RMS parameters:
- From the Home (RMS) page, use Right / OK button to navigate to RMS.
- Press the Up or Down button to navigate to the next RMS parameter.
- Press Left button to exit.
The navigation of RMS parameters:
The list of RMS parameters are as follows:
-
Per-phase and average voltage (line-to-line, line-to-neutral)
-
Per-phase and average current, and neutral current (calculated)
-
Per-phase and average power factor
-
Per-phase and total power (VA, W, VAR)
-
System frequency
-
Revolutions per minute (RPM)
-
Unbalance (voltage, current)
-
Per phase load percentage
-
Per phase angle (between voltage and current)