GEX7903902-00

Timer

The meter supports meter on hours and load run hours (only Utility, Alternate source and Total).

The timer data can be read through register map.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?