GEX7903902-00

Terminal covers

The voltage and current terminal covers help prevent tampering with the meter’s voltage and current measurement inputs.

The terminal covers enclose the terminals, the conductor fixing screws and a length of the external conductors and their insulation. These covers are secured by tamper-resistant meter seals. Ensure you push the cover upwards till you hear a click to make the cover stand.

These covers are included for meter models where sealable voltage and current covers are required to protect against tampering of current and voltage input signals.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?