Physical description
Front
The front panel has an LCD display with the following indicators and controls:
|
A |
Menu selection buttons |
|
B |
The Calibration LED blinks as per the energy updating rate |
|
C |
LCD |
|
D |
Voltage Line Indicators (L1, L2, L3), indicates when a phase line is ON. |
Rear
The rear of the digital meter with the following indicators and controls:
-
Six terminals for current, one in and one out per phase
-
Four terminals for voltage, for three phases and neutral
-
Two terminals for control power
-
Two terminals for the RS-485 communications port
|
E |
Voltage inputs |
|
F |
Control power |
|
G |
Retainer clip |
|
H |
RS-485 |
|
I |
Current inputs |