GEX7903902-00

Basic setup

Basic setup parameters is essential for accurate measurement and calculations. Use the Basic setup screen to define the electrical power system that the meter is monitoring.

To enter into Basic Setup:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Setup.
  4. Press OK.
  5. Enter the password. Default password is 0000.
  6. Press OK.
  7. Use Up or Down button to navigate to Basic Setup.
  8. Press OK to enter Basic Setup.
  9. Press Left button to exit Basic Setup after viewing parameters.
The navigation of Basic setup:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?