GEX7903902-00

Meter setup through RS-485

After the meter’s RS-485 port is configured and connected to the RS-485 network, you can use ION Setup to configure all other meter setup parameters.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?