GEX7903902-00

Overview

The section provides you information on viewing various parameter pages in the meter.

The meter navigation for GLDM3241 :

The meter navigation for GLEM3251 / GLEM3261 / GLEM3265 :

Information icons

Icons in the information area if the LCD display provides information such as what menu is selected.

Icon

Description

RMS

Energy and Non Reset Energy

Diagnostics

Old Energy

Reset

Setup

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.