GEX7903902-00

Diagnostics page

In Diagnostics, you can verify the meter information.

To view Diagnostics parameters:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Press the Up or Down button to navigate to the Diagnostics page.
  4. Press OK.
  5. Press the Up or Down button to navigate to the next Diagnostics parameter.
  6. Press Left button to exit.

The navigation of Diagnostics:

GLDM3241 / GLEM3251 / GLEM3261 / GLEM3265

Name on display

Description

Indicates that the display is operating correctly.

Serial number

Displays the meter serial number, for example 0500005174.

Meter Model

Displays the meter model number.

OS Version

Displays the operating system version number, for example OS 1.00.0.

RS Version

Displays the reset (boot code) version number, for example RS 1.00.0.

Diag Error

Displays the error codes of the meter for diagnostics.

Comm

Display the communication error code.

1, 19200, Even

Displays the ID, Baud, Parity.

On Hours

Displays the period for which the power meter's auxiliary supply is ON, regardless of the voltage and current inputs.

Power Fails

Display the number of times control power is interrupted.

System Edits

Display the count of system edit.

Lst Edt Time

Display the last edit time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?