GEX7903902-00

Meter configuration

Meter configuration can be performed through the display or ION Setup .

ION Setup is a meter configuration tool that can be downloaded for free at www.se.com ,If you already have an existing installation of ION Setup , it is recommended that you upgrade to the latest version in order to access new features or enhancements and properly configure features available on your device.

See the ION Setup online help or in the ION Setup device configuration guide. To download a copy, go to www.se.com and search for ION Setup device configuration guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?