GEX7903902-00

LED setup

NOTE: Applicable for (GLEM3251 / GLEM3261 / GLEM3265 ).

LED setup enables you to configure LED parameters. The meter’s display screen and buttons allow you to navigate and edit the required parameters.

To enter into LED Setup:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Setup.
  4. Press OK.
  5. Enter the password. Default password is 0000.
  6. Use Up or Down button to navigate to LED Setup.
  7. Press OK to enter LED Setup.
  8. Press Left button to exit LED Setup.
The navigation of LED setup:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?