GEX7903902-00

Setup screen menus

Setup screen enables you to configure various setup parameters.

To enter into setup:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Setup.
  4. Press OK.
  5. Enter the password. Default password is 0000.
  6. Press OK.
  7. Use Up or Down button to navigate to Setup pages.
  8. Press Left button to exit.

The navigation of setup:

Setup Parameters Description

Basic Setup

You can edit the basic setup parameters

LED Setup (GLEM3251 / GLEM3261 / GLEM3265 )

You can edit LED setup parameters

Comm Setup

You can edit Communication setup parameters

HMI Setup

You can edit HMI setup parameters

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?