GEX7903902-00

Applications

The meters can be used in various cost management and network management application. Some of the import applications are mentioned below.

Cost management

  • Energy accounting and balancing

  • Control panels

  • Power distribution boards

  • Original equipment manufacturers (OEMs)

  • Building management system

  • Panel instrumentation

  • Energy management system

Network management

  • Measurement of power factor

  • Phase angle between the voltage and current

  • % unbalance among voltage and current

  • Modbus RTU protocol RS-485 port for integration with energy management system

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?