DOCA0142EN-11

IO Modules

Description

The IO MODULES page displays the IO module input/output configuration. It displays six digital inputs and three digital outputs. The IO application control is possible only when the IO module is connected to a circuit breaker.

To open the IO MODULES page, navigate to MONITORING & CONTROL > IO MODULES.

Predefined Application

The number of the predefined application selected by the application rotary switch on the IO module is indicated in the following table:

Application Rotary Switch Position

Predefined Application

Description

1

Cradle management

Monitors the position of the circuit breaker in the cradle.

2

Circuit breaker operation

Controls the opening and closing of the circuit breaker by using the control mode (local or remote) and the inhibit close order.

3

Cradle management and Energy Reduction Maintenance Setting (ERMS)

Monitors the position of the circuit breaker in the cradle, monitors the position of inputs, and controls the ERMS mode of the circuit breaker.

4

Light and load control

Controls the light and load application.

5–8

Spare

9

Custom

Performs the user-defined applications with the IO module.

For more information, refer to the in DOCA0055•• Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide in the Related Documents section at the beginning of the guide.

List of Parameters in IO Module

The IO MODULES page displays the following parameters:

Parameter

Description

Setting

Inputs

Displays the six digital inputs configured in the IO module.

Outputs

Displays the three digital outputs configured in the IO module.

Label

Displays the assigned functions of the corresponding inputs or outputs.

Value

Displays the value of the six digital inputs and three digital outputs.

  • 1

  • 0

Forced

Displays the six digital inputs and three digital outputs are forced or not.

  • FORCED

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.