Hardware Description
Description

A |
Ethernet 1 and Ethernet 2 RJ45 communication ports |
B |
24 Vdc power supply terminal block |
C |
QR code to product information |
D |
Ethernet communication LEDs |
E |
Module status LED |
F |
Network status LED |
G |
Sealable transparent cover |
H |
Reset button |
I |
ULP status LED |
J |
Test button (accessible even with closed cover) |
K |
Locking pad |
L |
Device name label |
M |
Two RJ45 ULP ports |
N |
Grounding connection |
For information on installation, consult the instruction sheet available on the Schneider Electric website: QGH13473.
Mounting
The IFE interface mounts on a DIN rail.
24 Vdc Power Supply
The IFE interface must always be supplied with 24 Vdc.
It is recommended to use an UL listed and recognized limited voltage/limited current or a class 2 power supply with a 24 Vdc, 3 A maximum.
Ethernet Communication LEDs
The Ethernet communication dual color LEDs, indicate the status of the Ethernet ports ETH1 and ETH2.
LED Indication |
Status Description |
---|---|
OFF |
No power or no link |
Steady yellow |
10 Mbps, link established, and no activity |
Blinking yellow |
10 Mbps, ongoing activity |
Steady green |
100 Mbps, link established, and no activity |
Blinking green |
100 Mbps, ongoing activity |
Module Status LED
The module status dual color LED, indicates the IFE interface status.
LED Indication |
Status Description |
Action |
---|---|---|
OFF |
No power |
None |
Steady green |
IFE interface operational |
None |
Blinking green (250 ms ON, 250 ms OFF) |
Hidden control webpage available |
None |
Blinking green (500 ms ON, 500 ms OFF) |
IFE interface firmware corrupted |
Contact your local Schneider Electric service team for support. |
Blinking red (500 ms ON, 500 ms OFF) |
IFE interface in degraded mode |
Replace ULP module at the next maintenance operation. |
Steady red |
IFE interface out of service |
None |
Blinking green/red (1 s green, 1 s red) |
Firmware update in progress |
None |
Blinking green/red (250 ms green, 250 ms red) |
Self-test in progress |
None |
Network Status LED
The network status dual color LED, indicates the Ethernet network status.
LED Indication |
Status Description |
---|---|
OFF |
No power or no IP address |
Steady green |
Valid IP address |
Steady red |
Duplicated IP address |
Blinking green/red (250 ms green, 250 ms red) |
Self-test in progress |
Steady amber |
Error in IP configuration |
Modbus Address
The IFE interface accepts the Modbus address of the IMU to which it is connected.
The Modbus address is 255 and cannot be changed.
Locking Pad
The locking pad on the front panel of the IFE interface enables or disables the ability to send the remote control commands over the Ethernet network to the IFE interface, and to the other modules of the IMU
-
If the arrow points to the open padlock (default setting), remote control commands are enabled.
-
If the arrow points to the closed padlock, remote control commands are disabled.
The only remote control command that is enabled even if the arrow points to the closed padlock, is the set absolute time command.
Test Button
The test button has two functions, according to the duration of the button pressed.
Time Range |
Function |
---|---|
1–5 s |
Tests the connection between all the ULP modules for 15 s. |
10–15 s |
Activates the hidden configuration mode. NOTE: The hidden configuration is not activated
if the button is pressed for more than 15 s.
|
Reset Button
When the Resetbutton is pressed for 1–5 seconds, it forces the IP acquisition mode to the default setting (DHCP).
When the Reset button is pressed for more than 10 seconds, the IFE interface performs a reset of Security Administrator password to default setting (AAAAAAAA).
The following procedure describes the steps to reset the Security Administrator password to default setting:
-
Press the Reset button on the IFE interface for more than 10 seconds. The LED will blink fast in red (100 ms ON and 100 ms OFF).
-
After releasing the Reset button, the IFE interface is in Reset mode for 30 seconds and notifies the user to perform the reset to default settings. The LED will blink fast in red (100 ms ON and 100 ms OFF).
-
Press the Reset button on the IFE interface to confirm or wait for 30 seconds to cancel the reset.
-
After confirming the reset of Security Administrator password, the IFE interface reboots. All IFEsettings are reset to default settings, except the Reset administrator password counter and the general data.
ULP Status LED
The yellow ULP status LED describes the mode of the ULP module.
ULP LED |
Mode |
Action |
---|---|---|
Nominal |
None |
|
Conflict |
Remove extra ULP module |
|
Degraded |
Replace ULP module at the next maintenance operation |
|
Test |
None |
|
Non-critical firmware discrepancy |
Use EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions |
|
Non-critical hardware discrepancy |
||
Configuration discrepancy |
Install missing features |
|
Critical firmware discrepancy |
Use EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions |
|
Critical hardware discrepancy |
||
Stop |
Replace ULP module |
|
Power OFF |
Check power supply |