DOCA0142EN-10

SNMP Parameters

Manage IP Parameters

The IFE interface supports SNMP, allowing a network administrator to access remotely an IFE interface with an SNMP manager and to view the networking status and diagnostics of the IFE interface in the MIB-II format.

Parameter

Description

Setting

Manager One

Allows you to configure the IP address of SNMP manager one.

Manager Two

Allows you to configure the IP address of SNMP manager two.

System Contact

Allows you to configure the SNMP system contact name.

System Name

Allows you to configure the system name.

System Location

Allows you to configure the SNMP system location.

Read-only Community Name

Allows you to configure the SNMP read-only community name.

Public (default setting)

Read-write Community Name

Allows you to configure the SNMP read-write community name.

Private (default setting)

Trap

Allows you to trap the community name.

Alert (default setting)

NOTE: Only SNMP version 1 is supported.

Enabled Traps

Parameter

Description

Setting

Coldstart Trap

Generates a trap when the IFE interface is powered ON.

Warmstart Trap

Not supported

Linkdown Trap

Generates a trap when an Ethernet port communication link is disconnected.

Linkup Trap

Generates a trap when an Ethernet port communication link is reconnected.

Authentication Failure Trap

Generates a trap when an SNMP manager is accessing the IFE interface with incorrect authentication.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?