Statistics
Description
The IFE interface was last activated. If the power to the IFE interface is terminated or the device is reset due to a configuration change or other event, all cumulative values are reset to 0.
page shows the readings accumulated since theReset Procedure
Step |
Action |
Result |
---|---|---|
1 |
From the IFE menu bar, click . |
Opens the menu. |
2 |
From the menu, in the submenu, click . |
Opens the page. |
3 |
View the data. |
See the statistics for each group. |
4 |
Click . |
Resets the IFE cumulative diagnostic data to 0. |
Interpreting Ethernet Statistics
Global Statistic |
Description |
---|---|
|
Number of frames received |
|
Number of frames transmitted |
|
Resets the transmitted and received frames |
Statistic Per Port |
Description |
---|---|
|
Operational speed (10 Mbps or 100 Mbit/s) |
|
Current mode of operation (full duplex or half duplex) |
Interpreting Modbus TCP/IP Statistics
Statistic |
Description |
---|---|
|
Status of the connected Ethernet port |
|
Number of active connections |
|
Number of messages received |
|
Number of messages transmitted |
|
Resets the received and transmitted messages |
Interpreting System Statistics
Statistic |
Description |
---|---|
|
Status of the CPU:
|
|
Healthiness of the boot memory |
|
Healthiness of EEPROM |
|
Healthiness of the file system |
|
Healthiness of PHY 1 hardware |
|
Healthiness of PHY 2 hardware |
|
Healthiness of the execution memory |
Interpreting Date and Time Statistics
Statistic |
Description |
---|---|
|
Current date |
|
Current time |
|
Run time during the system power-up |
Interpreting Date /Time Synchronization
Statistic |
Description |
---|---|
|
|
|
Time elapsed since the last synchronization has happened |
|
Source of time with which the last synchronization has happened |
|
Last synchronization date |
|
Last synchronization time |
|
|
|
The following is the status of synchronization with SNTP:
|
Interpreting Modbus Serial Statistics
Statistic |
Description |
---|---|
|
A counter that increments each time a frame is sent. |
|
A counter that increments each time a frame is received. |
|
An error marked from the device or the response timeout. |
Interpreting ULP Statistics
Statistic |
Description |
---|---|
|
Number of CAN frames transmitted successfully |
|
Number of CAN frames received successfully |
|
Maximum number of CAN transmitted errors (TEC) |
|
Maximum number of CAN received errors (REC) |
|
CAN Bus off count |
|
Maximum number of bus off counts |
Interpreting File System Statistics
Statistic |
Description |
---|---|
|
Total amount of the IFE disk size in kilobytes |
|
Total amount of used disk size on the IFE disk in kilobytes |
|
Total amount of unused disk space on the IFE disk in kilobytes |
|
Amount of corrupted disk space on the IFE disk in kilobytes |
Interpreting TCP Port Connections Statistics
Statistics |
Description |
---|---|
|
Remote IP address |
|
Remote port number |
|
Number of messages transmitted |
|
Number of messages received |
|
Number of error messages sent |
|
Resets the transmitted and received messages |