Redundancy-RSTP Bridge
Description
The page displays the diagnostic data of RSTP bridge.
The users with installer or engineer roles can make changes to the Diagnostics page settings.
Navigation to the Redundancy-RSTP Bridge Page
To view the REDUNDANCY-RSTP BRIDGE page, click .
General Parameters
|
Parameter |
Description |
|---|---|
|
|
Status of RSTP feature. It is either enabled or disabled based on the configuration. |
|
|
Unique identifier of this Bridge. It is a combination of MAC address and Bridge Priority of this device. |
|
|
Unique identifier of the Root Bridge. Combination of MAC address and Root Bridge Priority of the Root device |
|
|
The port number that offers the lowest cost path from this bridge to the root bridge. NOTE: For the Root Bridge, the value is always 0. For other
devices, either 1 or 2.
|
|
|
The cost of the path to the root as seen from this bridge. |
|
|
Total number of topology changes detected by this bridge since the last reset counters. |
|
Click to reset the statistics values to 0. If the IFE interface is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0. |
|
Configured/Learned Parameters
|
Parameter |
Description |
|---|---|
|
|
The value of Hello Time configured at this Bridge. |
|
|
The actual Hello Time used by the bridge currently. This is the configured Hello Time of the Root Bridge. |
|
|
The value of Forward Delay configured at this Bridge. |
|
|
The actual Forward Delay used by the bridge currently. This is the configured Forward Delay of the Root Bridge. |
|
|
The value of Max Age Time configured at this Bridge. |
|
|
The actual Max Age Time used by the bridge currently. This is the configured Max Age Time of the Root Bridge. |