Redundancy-RSTP Ports
Description
The
page displays the diagnostic data of RSTP ports.The users with Installer or Engineer roles can consult the Diagnostics pages.
Navigation to the Redundancy-RSTP Ports Page
To view the
page, click .Port 1 and Port 2 Parameters
Parameter |
Description |
---|---|
|
Current state of the port. By default, it is disabled, blocking, and forwarding. NOTE: Other
states like listening, learning are intermediate states which are
not visible to the user.
|
|
Current role of the port in the ring. If the port state is disabled, the role can be either Root or Designated. If the port state is disabled (Ethernet link is down) then the Role is Unknown. |
|
The value of the port priority
is contained in Port Identifier. All ports of a bridge will have a
port identifier with NOTE: The below points
are provided for understanding the usage of port priority (port identifier).
|
|
The contribution of this port to the path cost of paths towards the Root bridge which includes this port. |
|
Total number of RSTP BPDUs received by this port since the last reset counters. |
|
Total number of RSTP BPDUs transmitted by this port since the last reset counters. |
|
Total number of Topology Change BPDUs received by this port since the last reset counters. |
|
Total number of Topology Change BPDUs transmitted by this port since the last reset counters. |
Click to reset to 0 the statistics values.If the IFE interface is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0. |