7EN02-0406-04

Insulation alarm time delay (Ins. Al. Delay)

Applicable for IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT.

In some applications you might want to delay the triggering of an alarm while certain machines are starting up, otherwise erroneous alarms could be triggered. You can set the threshold delay to filter these erroneous alarms.

The threshold delay is time filter. This delay can be used in harsh electrical systems to avoid false insulation alarms. The device does not report insulation fault that do not remain for a duration longer than the delay set up.

The allowed values for this parameter are from 0 s to 120 min. The default value is 0 s.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?