7EN02-0406-04

Voltage adaptor (V. Adapt)

Applicable for IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT.

You can use voltage adapter to monitor ungrounded power system with a rated voltage higher than 480 V AC/DC.

Two values are available for this parameter:

Value Advised Usage
None (Default) Use when the monitored ungrounded power system rated voltage is ≤ 480 V AC/DC.
VA1T Use when the monitored ungrounded power system rated voltage is > 480 V AC/DC and ≤ 1000 V AC/DC.

See Accessories for more information on voltage adaptors.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?