Reset
You can access the device reset parameters by selecting
.The reset parameters are Reset Logs, Reset Trend, and Factory Reset.
The parameters Reset Logs and Reset Trend are not applicable for IFL12C.
On performing reset of logs or trends, the existing logs or trend information is erased but the settings parameter value remains unchanged. On performing factory reset, the device restarts and automatic commissioning is initiated. Also, settings parameter values are reset to default.
The complete list of settings parameters, its default value, and allowed values are:
Parameter | Default Value | Allowed Values |
---|---|---|
Ins. Alarm |
IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT: 10 kΩ IFL12C: Low |
IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT: 0.2...200 kΩ IFL12C: Low, Medium, and High |
Ins. Al. Delay * | 0 s | 0 s...120 mn |
App * | Power C |
|
Filtering | 40s |
|
Frequency * | 50 Hz |
|
V.Adapt * | None |
|
Channel Name | CHANNEL – 1 to CHANNEL – 12 for 12 channels |
The length of the channel name is automatically adjusted depending on the character selection. For example, if the channel name contains only the character “W”, then the maximum length is 8 characters and if the channel name contains only the character “I”, then the maximum length is 18 characters. |
Ins. Al. Relay * | FS |
|
Ack. Al. Relay * | ON |
|
Test w.Relays * | ON |
|
Address | 1 | 1...247 |
Baudrate | 19200 |
|
Parity | Even |
|
Modify Password | 0000 | 0000...9999 |
Activation (Password) | OFF |
|
Contrast | 50% | 10...100% |
Backlight | 100% | 10...100% |
Screen Saver * | OFF |
|