Changing the channel name
- Navigate to .The CHANNEL NAME screen displays with the channel grid and a flashing dot on the channel 1 grid. This indicates the channel 1 is selected.
- Perform
any one of the following:
The CHANNEL NAME screen displays with the default name CHANNEL – 1 and the character C highlighted.
- Press
the
button.
The CHANNEL NAME screen displays and the default name is deleted and the screen is blank.
-
To delete the channel name, see Deleting the channel name.
-
To modify the channel name, press the
button.
The CHANNEL NAME screen displays and the highlighted character displays blank character.
-
- Press
the
button and navigate to the next character.
- Perform to update the selected character.
- Perform and for other characters.
- Press
the
button to confirm the channel name.
A Saved message displays. - Press the Esc button.The CHANNEL NAME screen displays with the channel grid and a flashing dot on the channel 1 grid. This indicates the channel 1 is selected.
- Perform to to change other channel names.