7EN02-0406-04

Alarm configuration

You can configure the insulation alarm threshold and delay to suit to the electrical applications you want to monitor.

You can access the device alarm parameters by selecting Menu > Settings > Ins.Alarm.

The alarm parameters are Ins. Alarm and Ins. Al. Delay.

The parameter Ins. Al. Delay is not applicable for IFL12C.

You can set the parameter values for all commissioned or uncommissioned channels *

To modify the parameter value, see Parameter modification using the display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?