About this manual
This manual is intended for use by designers, panel builders, installers, system integrators, and maintenance technicians who are related with ungrounded electrical distribution systems featuring insulation monitoring devices (IMDs) with fault locating devices.
Throughout the manual, the term “device” refers to IFL12C, IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT. All differences between the models, such as a feature specific to one model, are indicated with the appropriate model number or description. Throughout the manual, the term “IMD” refers to IM400, IM400L, and IM400C.
This manual assumes you have an understanding of insulation monitoring and locating and are familiar with the equipment and power system in which your device is installed.
This manual does not provide instructions on how to incorporate device data or perform device configuration using energy management systems or software.
Please contact your local Schneider Electric representative to learn what additional training opportunities are available for your devices.
Make sure you are using the most up-to-date version of your device’s firmware in order to access the latest features.
The most up-to-date documentation about your device is available for download from www.se.com.
Related documents
| Document | Number |
|---|---|
| Instruction Sheet: Vigilohm IFL12C, IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT Insulation Fault Locator | QGH34269 |
| Commissioning Guide: Vigilohm IFL12C, IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT Insulation Fault Locator | 7EN02-0416 |
| Vigilohm Catalog | PLSED310020EN |
| The IT earthing system: a solution to improve industrial electrical network availability - Application guide | PLSED110006EN |
| System earthings in LV (The schematics of earth links in LV (neutral modes) Cahier technique n° 172 ) | CT172 |
| The IT system earthing (unearthed neutral) in LV (The IT scheme (in isolated neutral) of the links to the earth in LV Cahier technique n° 178) | CT178 |