7EN02-0406-04

Insulation measurements

The device monitors the insulation per connected channel of ungrounded power system.

The device:

  • measures and displays:

    • the insulation resistance R (Ω) continuously,

    • the insulation capacitance C, which is the leakage capacitance of the distribution system to ground (μF), *

  • calculates and displays the impedance Zc (kΩ) associated with C for 12 channels. *

To view these values, navigate to Menu > Monitoring. To view each channel measurements, use the contextual menu buttons.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?