7EN02-0406-04

Hardware overview

Vigilohm IFL12MC / IFL12LMC / IFL12MCT / IFL12LMCT and IFL12C feature 5 and 4 terminal blocks respectively.
A Alarm relay
B Auxiliary power supply
C Product status LED
D Communication LED
E Menu button
F No alarm LED
G Esc button
H Alarm LED
I 3 contextual menu buttons
J

Label

NOTE: Scan the QR code to view the device documentation: QR code link

K RS-485 communication
L 12 toroid connections
M Voltage input *
N LCD screen
O Gasket
P Commercial reference and manufacturing data
Q

Specification Label

NOTE: Scan the QR code to view the device documentation: QR code link

R DIN mounting clip

Device commercial reference

Model Commercial reference
IFL12C IMDIFL12C
IFL12MC IMDIFL12MC
IFL12LMC IMDIFL12LMC
IFL12MCT IMDIFL12MCT
IFL12LMCT IMDIFL12LMCT
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?