7EN02-0406-04

I/O configuration

Applicable for IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT.

You can configure the relay parameters to suit the type of relay output information.

You can access the device I/O parameters by selecting Menu > Settings > I/O Config.

The I/O parameters are Ins. Al. Relay, Ack. Al. Relay, and Test w.Relays.

To modify the parameter value, see Parameter modification using the display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?