7EN02-0406-04

IM400 Configuration

You need to perform IM400 configuration to enable the device to work as expected.

Perform the following network settings on the IM400 (based on firmware version) to enable compatibility with the device:

NOTE: You need to perform these settings again when you perform factory reset on the IM400.

  1. Select Menu > Settings > Network.
  2. Set the value for the following network parameters and save:
    Parameter Value
    Firmware Version
    < 3.2.0 ≥ 3.2.0
    App Power C. or Control C. Power C. or Control C.
    Locating OFF IFL12
    V. Adapt None or PHT1000 None or PHT1000
    Injection Std <Not applicable>
    NOTE: See IM400 user manual for information on modifying parameters.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?