7EN02-0406-04

Auto test sequence

During auto test, the device’s indicator lights illuminate and information is shown on the display.

The following LEDs turn ON in sequence and turn OFF after the predefined time:

  1. Alarm Orange

  2. No Alarm Green

  3. Product Status Red

  4. Product Status Green

  5. Communication Orange

The relay toggles. See Test with relays for information on performing auto test with relays.

  • If the auto test is successful, the following screen appears for 3 seconds and a status screen is displayed:

  • If the auto test fails, the Product Status LED turns ON and a message is displayed to indicate that the product is malfunctioning. Disconnect the auxiliary power supply of device and reconnect. If the fault persists, contact technical support.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?