7EN02-0406-04

Insulation alarm (Ins. Alarm) thresholds

You can set the threshold value as per the level of insulation of the application you monitor.

The allowed values for this parameter for IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT are from 0.2 kΩ to 200 kΩ. The default value is 10 kΩ. This value can be set for 12 channels individually or together.

The allowed values for this parameter for IFL12C are Low, Medium, and High. The default value is Low. This value is common for all 12 channels.

When the device is powered up, it retrieves the last insulation alarm threshold values recorded.

An insulation alarm is cleared when the insulation level reaches 20% above the threshold.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?