7EN02-0406-04

Language

The device supports 8 languages for HMI display.

The list of languages supported by the device HMI are as follows:

  • English (Default)

  • French

  • Spanish

  • Russian

  • Chinese

  • Italian

  • German

  • Portuguese

To set the language, navigate to Menu > Language. To modify the parameter value, see Parameter modification using the display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?