7EN02-0406-04

Frequency

Applicable for IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT.

You can set the rated frequency of the monitored application.

Four values are available for this parameter:

  • 50 Hz (Default)

  • 60 Hz

  • 400 Hz

  • DC

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?