Access to Link150 Webpages
Supported Web Browsers
Browser |
Version with Windows XP |
Version with Windows Vista |
Version with Windows 7 |
---|---|---|---|
Internet Explorer |
IE 8.0 |
IE 9.0 |
IE 10.0 |
Firefox |
15.0 |
20.0 |
20.0 |
Chrome (recommended) |
24.0 and later |
24.0 and later |
24.0 and later |
First Access to the Link150 Webpages
The Link150 gateway name should be configured during the first access to the Link150 webpages.
![]() |
---|
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY,
AND CONFIDENTIALITY
Change default passwords at first use to help prevent
unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The procedure to access the Link150 webpages for the first time depends on the operating system of a PC:
-
Windows Vista, Windows 7, or newer operating systems
-
Windows XP or older operating systems
-
The Link150 device has a self-signed security certificate and by default it is in HTTPS enabled mode.Therefore, connecting to the Link150 interface displays a security message. Before accepting, confirm that communication with the Link150 has been established.
-
HTTPS Redirection is enabled by default. It is recommended to leave this setting enabled to secure communications between PC and the Link150 gateway.
First Access Through PC with Windows 7, Windows Vista, or Newer Operating Systems
Step |
Action |
---|---|
1 |
Disconnect the PC from the local area network (LAN) and switch off Wi-Fi if any. |
2 |
Connect an Ethernet cable from the PC to the Link150 gateway or to the Ethernet switch inside the panel. NOTE: Perform this action when the device goes to fallback
ip.
|
3 |
Open web browser. |
4 |
Click and the appears in the list of devices.NOTE: If the Link150-name is not displayed in the
list of devices in , verify that the PC Link150 are connected through the
router.
|
5 |
Double-click the selected . The login page automatically opens in the browser.NOTE:
|
6 |
Enter NOTE: The user
name and password are case-sensitive. The Administrator user name cannot be changed as it is a default user name for administrator
role.
|
7 |
To change the default password, click under Administrator user name.The Password Modification page is displayed. |
8 |
Enter , , and , and then click . |
9 |
To locate the Link150-XXYYZZ, select the menu, go to submenu, and then turn ON the toggle key.The RS485 LED of the selected Link150-XXYYZZ blinks for 15 seconds with 1 s ON and 1 s OFF (test mode). |
10 |
To name the Link150 gateway name. , select the menu, go to submenu, click , go to , and then enter in box and click to set the |
11 |
Write the Link150 name on a blank device name label and stick it on the existing one. |
-
Follow the preceding procedure when link150 gateway goes to fallback IP due to duplicate IP detection or due to any other case.
-
XXYYZZ are the last 3 bytes of the MAC address in hexadecimal format.
-
Check the firewall settings if DPWS is not enabled.
First Access Through PC with Windows XP or Older Operating Systems
Step |
Action |
---|---|
1 |
Disconnect your local PC from all networks (LAN) and switch off Wi-Fi if any. |
2 |
Connect an Ethernet cable from the PC to the Link150 gateway. NOTE: Perform this action when the device goes to fallback
ip.
|
3 |
Start Internet Explorer 8, Mozilla Firefox 15, Chrome 24 (or later versions). NOTE: The
PC automatically uses the default 169.254.#.# (#=0–255) and
the default subnet mask 255.255.0.0.
|
4 |
In the address box, type Example: For the Link150 gateway with the MAC address 00-B0-D0-86-BB-F7 or 0-176-208-134-187-247 in decimal, type 169.254.187.247 in the address box. |
5 |
Press , the login page automatically opens in the browser. |
6 |
Enter NOTE: The user
name and password are case-sensitive. The Administrator user name cannot be changed as it is a default user name for administrator
role.
|
7 |
To change the default password, click under Administrator user name.The Password Modification page is displayed. |
8 |
Enter , , and , and then click . |
9 |
To locate the Link150-XXYYZZ, select the menu, go to submenu, and then turn ON the toggle key.The RS485 LED of the selected Link150-XXYYZZ blinks for 15 seconds with 1 s ON and 1 s OFF (test mode). |
10 |
To name the Link150 gateway name. , select the menu, go to submenu, click , go to , and then enter in box and click to set the |
11 |
Write the Link150-name on a blank device name label and stick it on the existing one. |
-
Follow the preceding procedure when link150 gateway goes to fallback IP due to duplicate IP detection or due to any other case.
-
XXYYZZ are the last 3 bytes of the MAC address in hexadecimal format.
Access to Webpages
Follow the Network Discovery, Name Browsing, and IP Address Browsing process to access the webpages.
Webpage access depends on the IT infrastructure.
Network Discovery
Follow the below procedure to access the Link150 webpages after the Link150 gateway name has been configured.
Step |
Action |
---|---|
1 |
Connect the Link150 gateway or the Ethernet switch inside the panel to the local area network (LAN). |
2 |
Connect the PC to the local area network (LAN). |
3 |
Click Link150-name gets displayed in the list of devices. . TheNOTE: If the Link150-name is not displayed in the list of devices in . Verify that
the PC Link150 are connected through the router.
|
4 |
Double-click the Link150-name.The login page automatically opens in the browser. |
Name Browsing
DNS server is mandatory to browse by name. For more details about DNS, refer to DNS.
Step |
Action |
---|---|
1 |
Connect the Link150 gateway or the Ethernet switch inside the panel to the local area network (LAN). |
2 |
Connect the PC to the local area network (LAN). |
3 |
Start the web browser. |
4 |
In the address box, type the Link150-name that is written on the sticker located on the front face of the selected Link150 gateway. |
5 |
Press and the login page automatically opens in the browser.NOTE: If the Link150-name does
not appear in the list of devices in . Verify that the PC Link150 are connected through the router.
|
IP Address Browsing
In IP Address Browsing, IP configuration can be done manually or it gets configured through DHCP or BootP.
Step |
Action |
---|---|
1 |
Connect the Link150 gateway or the Ethernet switch inside the panel to the local area network (LAN). |
2 |
Connect the PC to the local area network (LAN). |
3 |
Start the web browser. |
4 |
In the address box, enter the IP address given by the IT administrator. |
5 |
Press and the login page automatically opens in the browser.NOTE: If the login page in the web browser does not open
or does not display correctly, verify the path. For example: In the
Internet Explorer browser, verify that
are checked. |