D3349896_02

Adding Device to Favorites

You can mark devices as favorites and access them directly from the Home screen in the Favorites section.

  1. On the Home screen, locate the device which you want to mark as a favorite.

  2. Tap the device. The control screen appears.

  3. Tap at the top right.

The device appears in the Favorites section on the Home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?