D3349896_02

Renaming Room & Floors

Renaming your rooms and floors allows you to create a personalized and organized space in the Mobile app. Also, you can control and manage devices based on their locations.


To change the room name:

  1. Tap > Floors & Rooms > tap on the room name.


    Room Details page appears.
  2. Tap next to your room name.


    Rename Room page appears.
  3. Enter a new name.

  4. Tap Save. The new room name is saved.

    NOTE: When you rename a room in the mobile app, it will immediately reflect in the Manager.

To view the floor level:

  1. Tap > Floors & Rooms > tap the Show Floors level toggle button.

    All available floor names and the number of rooms on each floor are displayed.


    Also, floor names are displayed in the Home screen.

To change the floor name:

  1. Tap > Floors & Rooms > tap the Show Floors level toggle button. Floors & Rooms page appears.

  2. Tap on the floor name. Floor Details page appears.

  3. Tap next to your floor name. Rename Floor page appears.

  4. Enter a new name.

  5. Tap Save . The new floor name is saved.

    NOTE: When you rename a floor in the mobile app, it will immediately reflect in the Manager.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?