D3349896_02

Home Management

You can link multiple homes linked to your app account and add additional users to access your home.

For example:

  • If you have two homes, you can avoid using different accounts to access it (Adding New Home).

  • Each family member can create their own account so the parent does not have to share their credentials (Enable Access to Your Home).

  • Homeowners can enable permanent or time-limited remote access for maintenance(Enable Access to Your Home).

There are three ways to access the Home Management section:

  • Tap > Home Management > select the home you want to manage.

    or,

  • On the Home screen, tap your home name at the top center of your screen > select your home from the available homes list.

    or,

  • On the Home screen, tap your home name at the top center of your screen > tap Home Management > select the home you want to manage.

In the Home Management section, you can:

  1. Edit the home name:

    • Tap your home > tap > edit the name > tap Confirm.

  2. Edit the address:

    • Tap your home > tap Home address > type the address > tap Next > tap Submit.

      NOTE: The address/location provided will be used to display weather updates in Weather Panel on the Home page.
  3. Remove home from your account:

    • Tap your home > tap Remove Home > Confirm.

  4. Manage access:

    • Tap your home > tap Manage access > select the access request you want to manage > edit parameters (ROLE, ACCESS TO ROOMS, ACCESS PERIOD, Remove access) > tap Update access/Remove access.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?