D3349896_02

General Control

Info 1

Info 1 widget displays the values of the object assigned. It displays the current indoor or outdoor temperature, reminders for daily tasks or important events.

  1. On the Home screen, tap the room in which you want to view the information.

Info 2

Info 2 widget displays the values of the object assigned. It displays the error message and status from various devices configured.

  1. On the Home screen, tap the room in which you want to view the information.

Bellpress

The Bellpress is used for the momentary activation of a load. To activate/deactivate the load:

  1. On the Home screen, tap the room in which you want to activate the doorbell function.

  2. Tap PRESS to activate the load.

    • Green () indicates doorbell function is activated.

    • Black () indicates doorbell function is deactivated.

Enable Preset

The Enable Preset serves to set the configured devices to pre-determined value. To activate/deactivate the preset level:

  1. On the Home screen, tap the room in which you want to activate/deactivate the preset level.

  2. Tap on the widget, the Enable Preset control screen appears.

  3. Tap on any of the configured preset value to set the preset level.

    • Preset value in green indicates, preset level is activated.

    • Preset value in black indicates, preset level is deactivated.

Two-State Enable

Two-State Enable widget is used to set the state of a load. To control the Two-State Enable function:

  1. On the Home screen, tap the room in which you want to control the function.

  2. Tap Start to set the state of a load.

  3. Tap Stop to unset the state of a load.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?