D3349896_02

Scene Control

Scene Trigger

The Scene Trigger is used to set a scene, enabling the adjustment of multiple lights to predetermined levels simultaneously. To activate a scene:

  1. On the Home screen, tap the room in which you want to activate a scene.

  2. Tap SET SCENE to execute all the predefined actions associated with the scene.

    • Green indicates scene is triggered.

    • Greyed out indicates scene is not triggered.

Local Scene Controller

The Local Scene Controller is used for triggering multiple lights to predefine labels simultaneously. To set the Local Scene Controller:

  1. On the Home screen, tap the room in which you want to activate a local scene.

  2. Tap SET SCENE to trigger the scene.

    • Green indicates scene is triggered.

    • Greyed out indicates scene is not triggered.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?