D3349896_02

Creating User Account and Logging In

Once the professional installer sets up the controller, they will hand it over to the homeowner. Subsequently, the homeowner can login into the mobile app using the registered email address/password. To additionally create any account for the Clipsal C-Bus manager mobile app, follow the below steps:

  1. On the welcome screen, tap Get started.

  2. On the login screen, tap Register to create an account.

  3. Fill in the Registration form.

  4. Read the Privacy notice and then accept the Terms of use.

  5. Tap Continue.

An e-mail with a verification link will be sent to your e-mail address. Click the link and verify your account. (The link expires in 24 hours)

NOTE: After successfully creating your account, log in to the app with your credentials.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?