D3349896_02

Blind Control

Change Over Relay

The Change Over Relay widget is designed to perform the actions such as opening, pausing, and closing electric curtains, blinds, and shutters.

  1. On the Home screen, tap the room in which you want to control the Change Over Relay.

  2. Tap on the widget, the Change Over Relay control screen appears.

  3. Tap to pause the shutter.

  4. Tap to close the shutter.

  5. Tap to open the shutter.

Shutter Relay Vertical

Shutter Relay Vertical is used to control the movement of vertical blinds or shutters, enabling you to adjust them according to preference.

  1. On the Home screen, tap the room in which you want to control the Shutter Relay Vertical.

  2. Tap on the widget, the Shutter Relay Vertical control screen appears.

  3. Use the vertical level slider to control the operation of electric curtains, blinds, and shutters individually.

  4. Tap to pause the shutter.

  5. Tap to close the shutter.

  6. Tap to open the shutter.

Shutter Relay Horizontal

Shutter Relay Horizontal is used to control the movement of horizontal blinds or shutters, enabling you to adjust them according to your preference.

  1. On the Home screen, tap the room in which you want to control the Shutter Relay Horizontal.

  2. Tap on the widget, the Shutter Relay Horizontal control screen appears.

  3. Use the horizontal level slider to control the operation of electric curtains, blinds, and shutters individually.

  4. Tap to pause the shutter.

  5. Tap to close the shutter.

  6. Tap to open the shutter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?