D3349896_02

Moments

Moment allows you to group multiple actions that are usually performed together.

Moments are created and edited in the Automations section.

  1. On the Home screen (Home Screen), tap .

  2. Select the Moments tab.

    NOTE: A moment will only set the status of devices. To transition the affected devices to a different status, you must either change it manually or create a reversing moment.

The widgets supported by the Moment are Light Switch, General Switch, Socket Switch, General Lighting Dimmer, AC Switch, Fan Switch, Shutter Relay Vertical, and Shutter Relay Horizontal.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?