D3349896_02

Rearranging Rooms on the Home Screen

By default, rooms on the Home screen are displayed in the following order (left to right):

  • Favorites

  • All

  • Rooms in alphabetical order


To rearrange rooms:

  1. You can either:
    • Tap > tap Floors & Rooms .

      or,

    • On the Home screen at the end of the room list, tap > Room Settings > Floors & Rooms.

  2. Tap .

  3. Long press the room name, then drag and drop the room name in the desired location.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?