D3349896_02

Edit Moments

To edit the Moment:

  1. On the Home screen, tap .

  2. Go to Moments, locate the Moment you want to edit and tap .

  3. On the Moment editor page, you can :

    • Change the icon of your Moment.

    • Change the name.

    • Change the desired state of a device (tap the device to open the device control screen).

    • Add more devices to the Moment (tap Add Actions).

    • Remove a device from the Moment (swipe the device left and tap ).

  4. Tap Save to save the changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?