D3349896_02

Using the Devices

Using the Clipsal C-Bus manager mobile app, you can control the device according to your preferences. The following table describes which widget to use for the required functionality.

Lighting Control

Light Switch

General Switch

Socket Switch

General Lighting Dimmer

Lighting Status

Lighting Preset

Blinds Control

Change Over Relay

Shutter Relay Vertical

Shutter Relay Horizontal

Climate Control

Fan Switch

AC Switch

Fan Controller

Scenes Control

Scene Trigger

Local Scene Controller

General Control

Info 1

Info 2

Bellpress

Enable Preset

Two-State Enable

Other Widgets

Alarm Panel

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?