D3349896_02

Lighting Control

Light Switch

You can control the lights using the Light Switch.

  1. On the Home screen, tap the room in which you want to control the lights.

  2. Tap to turn on the lights.

  3. Tap to turn off the lights.

  4. Tap on the Lights widget, the Light Switch control screen appears.

  5. Tap to turn on the connected lights.

  6. Tap to turn off the connected lights.

General Switch

You can control the lights using the General Switch.

  1. On the Home screen, tap the room in which you want to control the lights.

  2. Tap to turn lights on.

  3. Tap to turn lights off.

  4. Tap on the widget, the General Switch control screen appears.

  5. Tap to turn on/off the connected lights.

Socket Switch

You can control the power of the connected device using the Socket Switch.

  1. On the Home screen, tap the room in which you want to control the Socket Switch.

  2. Tap to turn on the lights.

  3. Tap to turn off the lights.

  4. Tap on the widget, Socket Switch control screen appears.

  5. Tap to turn on/off the connected lights power.

General Lighting Dimmer

You can adjust the brightness of the lights in a room and create different lighting moods.

  1. On the Home screen, tap the room in which you want to control the General Lighting Dimmer.

  2. Tap to switch General Lighting Dimmer on.

  3. Tap to switch General Lighting Dimmer off.

  4. Tap on the widget, the General Lighting Dimmer control screen appears.

  5. Tap to turn on the General Lighting Dimmer.

  6. Tap to turn off the General Lighting Dimmer.

  7. Drag the level slider up/down (you can control the level of a load from 1% to 100%) to increase/decrease the brightness.

Lighting Status

You can view the current status of a specific light.

  1. On the Home screen, tap the room in which you want to view the Lighting Status.

  2. View the light bulb icon to check light status.

Lighting Preset

You can control the Lighting Preset by establishing the load at a predetermined level ranging from 0% to 100%.

  1. On the Home screen, tap the room in which you want to control the Lighting Preset.

  2. Tap on the widget, the Lighting Preset control screen appears.

  3. You can set the desired level.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?