D3349896_02

Climate Control

Fan Switch

You can control the ceiling fans using Fan Switch.

  1. On the Home screen, tap the room in which you want to control the Fan Switch.

  2. Tap to switch on the fan.

  3. Tap to switch off the fan.

  4. Tap on the widget, the Fan Switch control screen appears.

  5. Tap to turn on the fan.

  6. Tap to turn off the fan.

Air Conditioner Switch

Air Conditioner (AC) Switch is a device that allows remote or automated control of air conditioning units.

  1. On the Home screen, tap the room in which you want to control the AC Switch.

  2. Tap to switch on the AC.

  3. Tap to switch off the AC.

  4. Tap on the widget, the AC Switch control screen appears.

  5. Tap to turn on the AC.

  6. Tap to turn off the AC.

Fan Controller

Fan Controller enables remote control of adjusting the fan speed.

  1. On the Home screen, tap the room in which you want to control the fan speed.

  2. Tap on the widget, the Fan Controller control screen appears.

  3. Tap to turn on the Fan Controller.

  4. Tap twice to increase the fan speed.

  5. Tap to decrease the fan speed and to turn off Fan Controller.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?