D3349896_02

Timers

You can add and configure a Timer for the widget. A Timer automates actions by triggering the device directly from the widget when required. You can play, pause, cancel, and activate or deactivate the timer, but you cannot delete it. Timers are set to run specific functions for a defined duration.

Below are the common applications for automating devices using Timer feature:

  • Activating sprinklers (Example: You can set the Timer for the sprinkler to run for 1 hour and it will automatically turn off after the set time.)

  • Running bathroom fans for a limited time

  • Controlling hallway lights to turn off automatically

  • Managing climate control systems based on time intervals

Timer feature is supported for the following widgets:

  • Light Switch (Single)

  • Socket Switch

  • General Switch

  • Lighting Preset

  • Fan Switch

  • AC Switch

  • Fan Controller

  • Two State Enable
  • Scene Trigger

  • General Lighting Dimmer (Single)

  • Enable Preset

Light Switch

You can control the lights using the Light Switch.

  1. On the Home screen, tap the room in which you want to control the lights.

  2. Tap to turn on the lights.

  3. Tap to turn off the lights.

  4. Tap on the Lights widget, the Light Switch control screen appears.

  5. Tap to turn on the connected lights.

  6. Tap to turn off the connected lights.

  7. Tap Add Timer. The Add Timer page appears.

    To set the Timer for a widget:

    • Select the hour you want to run the Timer from the Hours drop-down list.

    • Select the minutes you want to run the Timer from the Minutes drop-down list.

    • Select the seconds you want to run the Timer from the Seconds drop-down list.

  8. Turn on the Activate Timer toggle switch to activate the timer.

    NOTE: You can activate or deactivate the Timer using the Activate Timer toggle switch, however, you cannot delete it. When de-activated, the Timer will no longer appear in the widget, and the widget will continue its normal operation, such as turning On or Off.
  9. In the Functions section:

    • Select the return level from the Return Object Value drop-down list. This is the state the widget will return to after the Timer finishes.

    • Select the target level from the Target Object Value drop-down list. This is the state the widget will go to when the Timer starts running.
    • Example : If you have set 1 hour on the Timer, when the Timer is activated the night lamp will immediately go to the Target Object Value (OFF).

      After 1 hour, the lamp will go back to the Return Object Value (ON).
  10. Tap Save to save the Timer details. Once saved, Timer is added to the widget.

  11. Tap to run the Timer. The object will move to the target level.

  12. Tap to reset the Timer to its full preset duration and start counting down again from the beginning. If the Timer is running or has finished, it restarts the cycle while the object value remains unchanged.

  13. Tap to stop/cancel the Timer and go back to its original state. The object remains at its current level, and the Timer will stop. No further changes occur unless the Timer is started again.
  14. Tap to pause the Timer at any time (the Timer countdown stops temporarily). The object’s current level remains unchanged. No further change occurs until the Timer is resumed. Pause button appears only when the Timer is running.

    Once Timer is added, the widget appears in the home page as shown below:

    NOTE: You can play or pause the Timer from the home page also.
  15. To edit the Timer, tap in the Timer screen to navigate to the edit Timer details screen.

    Make necessary changes and tap Update. The details are updated.

General Switch

You can control the lights using the General Switch.

  1. On the Home screen, tap the room in which you want to control the lights.

  2. Tap to turn lights on.

  3. Tap to turn lights off.

  4. Tap on the widget, the General Switch control screen appears.

  5. Tap to turn on/off the connected lights.

  6. Tap Add Timer. For more information on Add Timer refer Light Switch.

Socket Switch

You can control the power of the connected device using the Socket Switch.

  1. On the Home screen, tap the room in which you want to control the Socket Switch.

  2. Tap to turn on the lights.

  3. Tap to turn off the lights.

  4. Tap on the widget, Socket Switch control screen appears.

  5. Tap to turn on/off the connected lights power.

  6. Tap Add Timer. For more information on Add Timer refer Light Switch.

General Lighting Dimmer

You can adjust the brightness of the lights in a room and create different lighting moods.

  1. On the Home screen, tap the room in which you want to control the General Lighting Dimmer.

  2. Tap to switch General Lighting Dimmer on.

  3. Tap to switch General Lighting Dimmer off.

  4. Tap on the widget, the General Lighting Dimmer control screen appears.

  5. Tap to turn on the General Lighting Dimmer.

  6. Tap to turn off the General Lighting Dimmer.

  7. Drag the level slider up/down (you can control the level of a load from 1% to 100%) to increase/decrease the brightness.

  8. Tap Add Timer. The Add Timer page appears.

    For more information on Add Timer refer Light Switch.
    NOTE: For General Lighting Dimmer, the Return Ramp Rate and Target Ramp Rate drop-down options are also applicable in the Functions section.
  9. In the Functions section:
    • Select the time (instantaneous, seconds and minutes) from the Return Ramp Rate drop-down list. This defines how quickly the widget moves back to the return object value when the Timer ends.

    • Select the time (instantaneous, seconds and minutes) from the Target Ramp Rate drop-down list. This defines how quickly the widget moves to the target object value when the Timer starts.

Lighting Preset

You can control the Lighting Preset by establishing the load at a predetermined level ranging from 0% to 100%.

  1. On the Home screen, tap the room in which you want to control the Lighting Preset.

  2. Tap on the widget, the Lighting Preset control screen appears.

  3. You can set the desired level.

  4. Tap Add Timer. The Add Timer page appears.

    For more information on Add Timer refer Light Switch.
    NOTE: For Lighting Preset, the Return Ramp Rate and Target Ramp Rate drop-down options are also applicable in the Functions section.
  5. In the Functions section:
    • Select the time (instantaneous, seconds and minutes) from the Return Ramp Rate drop-down list. This defines how quickly the widget moves back to the return object value when the Timer ends.

    • Select the time (instantaneous, seconds and minutes) from the Target Ramp Rate drop-down list. This defines how quickly the widget moves to the target object value when the Timer starts.

Fan Switch

You can control the ceiling fans using Fan Switch.

  1. On the Home screen, tap the room in which you want to control the Fan Switch.

  2. Tap to switch on the fan.

  3. Tap to switch off the fan.

  4. Tap on the widget, the Fan Switch control screen appears.

  5. Tap to turn on the fan.

  6. Tap to turn off the fan.

  7. Tap Add Timer. For more information on Add Timer refer Light Switch.

Air Conditioner Switch

Air Conditioner (AC) Switch is a device that allows remote or automated control of air conditioning units.

  1. On the Home screen, tap the room in which you want to control the AC Switch.

  2. Tap to switch on the AC.

  3. Tap to switch off the AC.

  4. Tap on the widget, the Air Conditioner Switch control screen appears.

  5. Tap to turn on the Air Conditioner.

  6. Tap to turn off the Air Conditioner.

  7. Tap Add Timer. For more information on Add Timer refer Light Switch.

Fan Controller

Fan Controller enables remote control of adjusting the fan speed.

  1. On the Home screen, tap the room in which you want to control the fan speed.

  2. Tap on the widget, the Fan Controller control screen appears.

  3. Tap to turn on the Fan Controller.

  4. Tap twice to increase the fan speed.

  5. Tap to decrease the fan speed and to turn off Fan Controller.

  6. Tap Add Timers. For more information on Add Timer refer Light Switch.

Scene Trigger

The Scene Trigger is used to set a scene, enabling the adjustment of multiple lights to predetermined levels simultaneously. To activate a scene:

  1. On the Home screen, tap the room in which you want to activate a scene.

  2. Tap SET SCENE to execute all the predefined actions associated with the scene.

    • Green indicates scene is triggered.

    • Greyed out indicates scene is not triggered.

  3. Tap Add Timers. For more information on Add Timer refer Light Switch.

Two-State Enable

Two-State Enable widget is used to set the state of a load. To control the Two-State Enable function:

  1. On the Home screen, tap the room in which you want to control the function.

  2. Tap ALL ON to set the state of a load.

  3. Tap ALL OFF to unset the state of a load.

  4. Tap Add Timers. For more information on Add Timer refer Light Switch.

Enable Preset

The Enable Preset serves to set the configured devices to pre-determined value. To activate/deactivate the preset level:

  1. On the Home screen, tap the room in which you want to activate/deactivate the preset level.

  2. Tap on the widget, the Enable Preset control screen appears.

  3. Tap on any of the configured preset value to set the preset level.

    • Preset value in green indicates, preset level is activated.

    • Preset value in black indicates, preset level is deactivated.

  4. Tap Add Timer. The Add Timer page appears.
    For more information on Add Timer refer Light Switch.
    NOTE: For Enable Preset, the Return Ramp Rate and Target Ramp Rate drop-down options are also applicable in the Functions section.
  5. In the Functions section:
    • Select the time (instantaneous, seconds and minutes) from the Return Ramp Rate drop-down list. This defines how quickly the widget moves back to the return object value when the Timer ends.

    • Select the time (instantaneous, seconds and minutes) from the Target Ramp Rate drop-down list. This defines how quickly the widget moves to the target object value when the Timer starts.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?