D3349896_02

Weather Panel

You can enable the Weather Panel during the final step of the registration process or in the Settings. The weather panel displays the weather updates for the address entered in the Home Management section. (Home Management).

To view the weather information on your Home page:

  1. Tap > Home Screen > Weather Panel > tap the Show Weather Panel toggle button.

  2. Tap Temperature Units and select °C or °F.

  3. Tap Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?